Edit USB/GPIB Interfaces

To edit properties of a USB/GPIB Interface Converter (Keysight 82357) that is connected to your PC:

  1. In Connection Expert, select the USB/GPIB interface from the list of instruments and interfaces that can be edited. These are specified in the list by type and VISA interface ID (for example, USB/GPIB interface GPIB0).
  2. Then click .

  3. Modify the interface properties (described in detail below) as needed.

  4. Click OK.

Notes:

  • Because USB/GPIB interface converters permit GPIB instruments to be connected to the PC (via the PC's USB port), they are treated as GPIB interfaces by VISA. Instruments connected via USB/GPIB interface have GPIB addresses and GPIB-style properties.
  • You can use multiple USB/GPIB interface converters on the same PC.
  • If you connected a USB/GPIB interface converter before you installed the Keysight IO Libraries Suite, you may need to disconnect the USB/GPIB interface converter from the computer and then re-connect it to complete the hardware installation.

To change the VISA implementation used on this interface, see VISA Conflict Manager.

Specify Connection Addresses

Connection Expert manages the default numbering used with the VISA interface ID, SICL interface ID, and logical unit properties. When configuring one of these properties, Connection Expert uses the next available integer value. For example, if the VISA interface ID GPIB0 is already in use on another interface, the default value for this interface becomes GPIB1.

Conflicts may occur between board numbers of different vendors' GPIB interfaces, particularly where these board numbers are set using different configuration tools (such as Keysight Connection Expert for Keysight interfaces and NI-MAX for National Instruments interfaces). Connection Expert scans for conflicts when new interfaces are detected, and renumbers Keysight interfaces if necessary.

To change another vendor's board numbers, you must use that vendor's configuration utilities (for example, NI MAX).

VISA Interface ID

A name that Connection Expert and VISA use to uniquely identify this interface.  The VISA interface ID for a USB/GPIB interface is of the form GPIBn, where n is an integer. The VISA interface ID is part of the addressing string used to open a VISA programming session to a GPIB instrument.

If you have GPIB interfaces from different vendors installed in your system, you may see conflicts if the same VISA interface ID is assigned (by different vendors' configuration tools) to more than one interface. See Board Number Conflict for details.

Note that the board number (used in Keysight 488 function calls) is the numeric part of the VISA Interface ID. For example, if the VISA interface ID of your interface is GPIB1, its board number is 1.

GPIB Address

The address of this interface on the GPIB bus. The GPIB address can be any integer from 0 to 30.  It is usually set to 21 if the GPIB interface is a system controller, or 20 if not a system controller.

An 82357 USB/GPIB interface converter must be the system controller; it does not support a non-controller mode. This means it controls talkers and listeners on the GPIB bus.

SICL Interface ID

A name that SICL uses to uniquely identify this GPIB interface. The default SICL interface ID is gpibn, where n is an integer. If you are not using the default SICL interface ID, enter a unique string of alphanumeric characters (it can also include the _ and - characters). The SICL interface ID can be a maximum of 31 characters long and must start with a letter. Remember this value and the logical unit number in order to address the GPIB interface properly in your SICL applications.

Logical Unit

An integer that can be used in place of the SICL interface ID in Keysight VEE and SICL applications.  The logical unit is not used by VISA.  

Auto-Discover Options

Auto-Discover Instruments Connected to This Interface

When the Auto-Discover check box is selected, the interface will find new instruments whenever it is scanned. When the check box is cleared, the interface does not discovery new instruments. The interface is scanned on startup of the PC, whenever you click Rescan All in Instruments view, and periodically in the background if Auto-Scan is enabled. (Auto-scan is not available on all interface types.)

Auto-discovery defaults on for USB/GPIB interfaces.

Auto-Scan Options

By default, auto-scan is on but will be disabled automatically if problems are detected. You can choose to specify that auto-scan is always on or always off for this interface.

If Auto-Discover is turned off (cleared), then the Auto-Scan setting has no effect and is disabled (grayed).

Do Not Auto-Scan For Instruments On This Interface

If you select this option, auto-scan is turned off. New instruments will be discovered, and disconnected instruments removed, only on PC startup and when you click Rescan All .

Always Auto-Scan For Instruments On This Interface

If you select this option, the Discovery Service will scan this interface for new instruments and disconnected instruments periodically.

Auto-Scan Unless a Problem Is Detected

This is the default setting. Auto-scan is enabled unless the Discovery Service detects an instrument or condition that may cause problems on auto-scan. For example, certain instruments go in remote mode when scanned, so if one of those instruments is detected, auto-scan is disabled on this interface.

If you select Auto-Scan Unless a Problem Is Detected, you will see a message indicating the current state of auto-scan (enabled or disabled). The message may also indicate the reason if auto-scan is disabled. If auto-scan is disabled, you can still look for new or disconnected instruments by clicking Rescan All .

The IO Libraries Suite auto-scan feature can cause certain instruments on GPIB interfaces to go into remote mode every 15 seconds. When the Discovery Service detects an affected instrument model, it automatically turns off auto-scan for the affected GPIB interface. For detailed information on this issue, see Instrument Discovery and Identification on Specific Interface Types.

In addition, some older instruments do not respond correctly to the SCPI identification query, *IDN? These instruments may experience problems when queried by the IO Libraries Suite. After two failures, IO Libraries Suite will stop sending *IDN? to that instrument until the next reboot or reconnect. You can prevent *IDN? from ever being sent to an instrument by manually adding the instrument and turning off its auto-identification property.

Keysight 488 Properties

Click the down arrow to expand the properties related to the Keysight 488 library.

Saving the Configuration

The OK button is enabled if you have made changes to the information in this view. When you have finished entering the information, click OK to save the configuration or Cancel to revert to the previous saved values.

See Also

About Instrument Discovery and Identification

How Do I Configure Keysight Board Numbers and Logical Units for Use with VEE?

82357B USB/GPIB Interface Converter User's Guide

Keysight VISA Help

You can access the VISA, VISA.NET, VISA COM, Keysight 488, and SICL documentation by selecting Documentation from the IO Control (select the icon on your taskbar ).

 

Search Keywords interface configuration, set up, setup, modify, change parameters