System Requirements

Ensure that the following minimum system requirements are met before you install and run PathWave Desktop Edition.

Operating System
  • Windows 10 (64-bit)
  • RedHat 7.6 (64-bit)
Processor

Intel Core i5 (or equivalent)

RAM

16 GB

Storage Drive

2.5 GB free space 

Screen Resolution

1280 x 800 pixels

IO Libraries Suite

2019 or later

Required for instrument connectivity. To download, visit http://www.keysight.com/find/iosuite.

NOTE

PathWave Visualization requires WebGL 2.0. On Linux, this requires a hardware accelerated OpenGL implementation (minimum v3.0). To verify your system meets the requirement, visit https://webglreport.com/?v=2. Windows is not affected.