Uninstall PathWave Desktop Edition

This section describes how to uninstall PathWave Desktop Edition.

NOTE

Uninstalling PathWave Desktop Edition does not remove the installed services. To uninstall a service, see Uninstall a Service.

Prerequisites

  • On Windows, ensure that you have administrative privileges.
  • On Linux, ensure that you have super user and sudo access.

Uninstall PathWave Desktop Edition from Windows

  1. Open Control Panel > Programs and Features.
  2. Select PathWave Desktop Edition and click Uninstall/Change.
  3. Click Yes  on the pop-up window to continue the uninstall.
  4. Click OK.

Uninstall PathWave Desktop Edition from Linux

  1. Open a Terminal window.
  2. Change directories to PathWave Desktop Edition installation directory. 
  3. Type the following command and press Enter.

    ./UninstallPathWave
  4. Click Yes on the pop-up window to continue the uninstall.
  5. Click OK.