Perform Self-Test
Ensure that the X8721A is actively connected to your PC (via USB) and that you have selected it as an instrument. Follow the instructions as indicated in the image to perform self-test.
WARNING
Two units of 50-Ohm terminations are required to properly run the self-test. Without these, it is possible that some of the RF related self-tests could produce false failures.
- Once you have launched the IoT Soft Front Panel, click the Utility view (wrench icon).
- In the Self Test section, you may select to only run a specific option from the drop-down list. The default selection will be to run all of the available tests.
- Click Run to start the test and follow the onscreen instructions. View the summary of the results as shown in the area marked below.