Install the Software

Keysight Event-Based Power Analysis Install Wizard

The Keysight Event-Based Power Analysis Install Wizard is a centralized application that contains the necessary software prerequisites for the X8712A IoT device battery life optimization solution. Download the latest Install wizard to access the new releases of the software packages.

  1. Go to www.keysight.com/find/KS833A2A for Keysight Event-Based Power Analysis Install Wizard. You will need to run and install this software.
  2. Run the installer and follow the on-screen instructions. Click Finish to complete the installation.
  3. If not already launched, double-click the shortcut created on your desktop to launch the Install Wizard.
  4. Select the software components as stated to install them in your PC.
  5. When the status reflects the latest version installed, you may close the Install wizard.

Uninstall Event-Based Power Analysis

  1. Click the Windows button and search for Control Panel.
  2. Under the Programs category, click 'Uninstall a program' and search for 'Keysight Event-Based Power Analysis'.
  3. Click Uninstall to remove the application.