Basic View
The Soft Front Panel Utility is a free software that you can use without a license to measure advertising interval, transmit power, and packet error rate for an Active Scan DUT.
The items are as described in the table below.
| Item | Information | Description |
|---|---|---|
| 1 | DUT Information |
Display the information about the selected DUT.
|
| 2 | TX power envelope |
To use this feature, you will need to set the Capture Depth (via Configuration panel) which uses the default value of 1000 ms. At the end of the single run, it will display the graph of Power (dBm) against the set duration. For more information about this setting and how to configure the Capture Depth setting, go to Bluetooth Low Energy Test Setup Configuration. Note: In IoT Soft Front Panel Utility, you will not be able to specify the frequency when measuring Tx Power Envelope. In addition, you will not be able to save and export raw data in CSV file. |
| 3 | Advertising interval | This will show the minimum, average, and maximum Advertising Intervals recorded in a single run. |
| 4 | Transmit power | This will show the averaged transmit power measurements for Advertising Channels (Channel 37, 38 and 39). |
| 5 | Packet error rate | This will show the averaged measurements for packet error rate. |