Multi-DUT Composite Test
This view displays the information acquired according to the number of DUT(s) in the shield box, subject to user's selection or the Multi-DUT HW option purchased. The settings required for this test are as described in Multi-DUT Settings.
To modify the display of information in the Multi-device Measurement Result Table, click the Show Column drop-down list and select the check boxes next to the categories as shown below.
| Category | Description |
|---|---|
| Friendly Name | Display the device name of the discovered device. |
| DUT Status | Display the status of the discovered device. |
| PER Quality | Display the quality of PER. |
| PER Mode |
Display the PER mode supported by the DUT.
|
| Advertising Interval (ms) |
Display the advertising interval acquired. |
| RSSI (dB) and Channels |
Display the Receiver Signal Strength Indicator (RSSI) value of the DUT. The DUT should have the highest RSSI value (dB) when placed in the shield box. When RSSI Channel is selected, it will show the respective RSSI values for Channel 37, 38, and 39. |
| TX Power and Channels |
Display the averaged TX Power (dBm) out of the Channel 37, 38, and 39. When TX Power Channel is selected, it will show the respective TX Power for each channel. |
| Active Scan PER and Channels |
Display the PER results (%) for Channel 37, 38 and 39. When Active Scan Channel is selected, it will show the respective PER results (%) for Channel 37, 38, and 39. |
| Advertising Data and Response Data (Hex) | Display the advertising and response data (hexadecimal) that is used during the communication between the DUT and the X8721A. |