Physical and Current Events
There are two types of events as shown in the Settings window below.
- Physical event
Channel 2 to 4 are known as Physical events, where these events are optional depending on the selected channels. The colors displayed corresponds to the channels labelled on the N6705C in Channels. - Current event
Other events derived from the current waveform (Channel 1) using zones are always valid when the program is running. The region is defined by the upper or lower zones of the data from Avg Channel 1.
The table below contains the details of each column with its priority are arranged from highest to lowest (top to bottom).
| Calculation Source | Label | Color | Definition |
|---|---|---|---|
| Ch 2 Pwr Det | DUT TX |
Light Green |
Synchronous comes from X8712AD, assign as DUT’s TX events with the highest priority. |
| Ch 2 Pwr Det | Pair TX |
Dark Green |
Synchronous comes from X8712AD, assign as Pairing TX or DUT RX events with second highest priority. |
| Ch 3 - VM | LED1 | Blue |
Select from VM, AM or 2Q-PS mode, synchronous from Channel 3. |
| Ch 4 - VM | LED2 | Purple |
Select from VM, AM or 2Q-PS mode, synchronous from Channel 4. |
| Ch1 - Battery | Standby | Pink |
Region or window defined by a minimum and maximum current of channel 1. Any values that fall within the window will be included. |
| Ch1 - Battery |
MCU |
Orange |
Same as Region 1 with a lower priority |
| Ch1 - Battery | Other | Red | Same as Region 1 with the lowest priority |
- When there are two events in the same zone, the software will prioritize the events listed towards the top of the Calculation Source table. The software will not take in consideration of the disabled channels as part of the Results.
- The channels that are disabled in software settings will be grayed out when you view this table.