Results
A summary of the results can be found below where its definition is as described in the table below.
| Settings | Description |
|---|---|
| Battery Life |
Estimated battery life in hours based on the amount of Charge by Event cycle time and battery capacity set. Battery Life = Battery Capacity (Ah) / Total Charge (Ah) * Cycle time (h). Note: This is based on an ideal battery. |
| Total Charge |
Current integration based on cycle time to measure charge capacity in Ampere per hour. Total Charge (Ah) = sum of all Channel 1 current data within cycle time * time interval / 3600 seconds |
| Cycle Time |
The time frame set in the Zoom From and To in the main chart. This is also known as the analysis time. |
| Max Current | Maximum current recorded in the area between the two line markers. The reading at the result panel is the maximum of the Current reading at the specified sampling rate and time interval settings. |
| Avg Current |
Average current recorded between the two line markers. Avg current = Total Charge (Ah) / Cycle time (h). |
Click the Results button to view the detailed results according to the events in a separate pop-up window.
| Settings | Description |
|---|---|
| Event and Source | The Name of the events and sources are as described in Physical and Current Events. |
| Occupied Time |
Display the occupied time in seconds and the percentage (%) of each event. This information is also illustrated in the bar chart according to the color of each label. |
| Charge Consumption |
Sorts synchronous physical or current events within cycle time in Charge by Event = Synchronous charge by events (Ah) / Total Charge (Ah) within cycle time * 100% |