User Interface Tour

This section introduces you to the graphical user interface (GUI) for IoT Soft Front Panel application. 

PathWave Desktop Edition Home

This section explains the commonly used features that you will use in the PathWave Desktop Edition.

Guided Tour

The Tour Guide feature guides you through the IoT Soft Front Panel for a quick understanding of the features and settings. Click the compass icon located at lower right corner of the software to show the description of the functions available in each view or page.

System Wide Controls

These are the generic controls that you can use across all the measurements in IoT Soft Front Panel.

IoT Soft Front Panel Utility

The Soft Front Panel Utility is a free software that you can use without a license to measure advertising interval, transmit (TX) power, and packet error rate. The IoT Soft Front Panel Utility also allows you to perform firmware upgrade and self test on your X8721A.

IoT Soft Front Panel Pro

With the XA8722A_SFP license, you will be able to see the average, minimum, and maximum values for TX power, packet error rate, and throughput measurements using IoT Soft Front Panel Pro. You will also be able to access the chart view for these capabilities in the side menu.

The IoT Soft Front Panel Pro covers the following radio formats, which you must select before running a measurement.