Bluetooth Low Energy Radio
This section describes the features and functions of IoT Soft Front Panel which you will use when working with a Bluetooth Low Energy DUT.
| Item | Features |
|---|---|
| 1 |
The controls here include the Configuration panel, radio and device selection, and instrument selection. The configuration settings are as described in Bluetooth Low Energy Test Setup Configuration. |
| 2 |
The side menu shows the names of each chart view in the IoT Soft Front Panel (require an XA8722A_SFP license):
Note: The chart views have their individual settings that are as described in Chart View Settings. |
| 3 |
This panel displays the following information about the selected DUT:
|
| 4 |
Measurement Results With the XA8722A_SFP license, you will be able to see the average, minimum, and maximum measurements in Bluetooth Low Energy Basic View. |
| 5 |
This is the SCPI log panel with the location of the file (in "UserLog-mm-dd-yyyy" format). You can drag the top of this panel to pull it down and expand the main view. |
| 6 |
You can find this compass icon at the same location throughout the software. Click the compass icon to show description of the functions available in each view or page. |