Copy Files and Folders

The File View enables you to copy the project files and folders from one folder to another within the PathWave file system. 

To Copy Files and Folders

  1. Click .
    The Open File view is displayed listing the files and folders in the project.
  2. Browse to the desired location.
  3. Use the checkbox to select the files and folders you want to copy.
    The file operation toolbar is displayed.

  4. Click Copy to.

  5. In the Copy Item(s) dialog box, browse to the desired location.

  6. Optional. Click New Folder if you want to copy the file to a new folder.

  7. Click Copy.
    The selected file(s) and folder(s) are copied to the specified folder.

See Also