Restore Deleted Files and Folders

The deleted files and folders are moved to the Recycle Bin and the File View allows you to restore these files and folders.

To Restore a Deleted File or Folder

  1. Click   > Recycle Bin.
    The Open File view is displayed listing the files and folders in the Recycle Bin.
  2. Browse to the desired location.
  3. Use the checkbox to select the files and folders from the list.
    The file operation toolbar is displayed.

  4. Do one of the following:
    • If you want to move the file, 
      1. Click Move to.
      2.  Browse to the desired location and click Move.
    • If you want to copy the file, 
      1. Click Copy to.
      2. Browse to the desired location and click Copy.
    • If you want to download the file to your local system, 
      1. Click Download.
      2. Browse to the desired location and click Save.

See Also