Open a File

You can open the files stored in a PathWave file system from the Project Tree or the File View.

NOTE

A file can be opened only if an associated service is available. For example, a test plan (.TapPlan) file can be opened only if you have installed the PathWave Test Automation service.

To Open a File from the File View

  1. Click .
    The Open File view is displayed listing the files and folders in the project.
  2. Browse to the desired location.
  3. Click the filename.
    The file is opened in the associated PathWave service.

To Open a File from the Project Tree

  1. In the Project Tree pane, browse to the desired file.
    If the Project Tree pane is hidden, click  on the home view.
  2. Double-click the file.
    The file is opened in the associated PathWave service.

See Also