Rename Files and Folders
The File View enables you to rename the project files and folders present in the PathWave file system.
To Rename a File or Folder
- Click
.
The Open File view is displayed listing the files and folders in the project. - Browse to the desired location.
-
Select the file or folder from the list.
The file operation toolbar is displayed.- The Rename option is disabled if more than one file or folder is selected.
- Use the checkbox to select the file and folder. Clicking on the file or folder name will open it.
-
Click Rename.
- In the Enter New Name dialog box, type the new name and click Rename.
The name of the selected file or folder is updated.