Move Files and Folders

The File View enables you to move the project files and folders from one folder to another within the PathWave file system. 

To Move Files and Folders

  1. Click .
    The Open File view is displayed listing the files and folders in the project.
  2. Browse to the desired location.
  3. Use the checkbox to select the files and folders from the list.
    The file operation toolbar is displayed.

  4. Click Move to.

  5. In the Move Item(s) dialog box, browse to the desired location.

  6. Optional. Click New Folder if you want to store the file in different folder.

  7. Click Move.
    The selected file(s) and folder(s) are moved to the specified folder.

See Also