Delete Files and Folders
The File View enables you to remove the project files and folders from the PathWave file system.
To Delete Files and Folders
- Click
.
The Open File view is displayed listing the files and folders in the project. - Browse to the desired location.
-
Use the checkbox to select the files and folders from the list.
The file operation toolbar is displayed. -
Click Delete.
- Click Recycle.
The selected file(s) and folder(s) are moved to the Recycle Bin.
To Permanently Delete Files and Folders
When you delete a file or folder, it is moved to the Recycle Bin. You can permanently delete a file or folder from the Recycle Bin.
If you permanently delete a fie or folder, you cannot recover it later.
- Follow the instructions to delete files and folders.
- Click Recycle Bin.
- Browse to the desired location.
-
Use the checkbox to select the files and folders from the list.
The file operation toolbar is displayed. -
Click Delete.
- Click Delete.
The selected file(s) and folder(s) are permanently deleted.
See Also
- View Files and Folders
- Search for Files and Folders
- Rename Files and Folders
- Copy Files and Folders
- Move Files and Folders
- Restore Deleted Files and Folders
- Upload a File
- Download a File
- Open a File
- Save a File